Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Configuring the Flashing of an Alarm

You configure an alarm to flash in the Alarms pane and Alarm view when it is triggered, so that the operator can see the alarm more easily.

To configure the flashing of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. Click the Presentation tab.

  3. Select Flashing to make the alarm flash in the Alarms pane and Alarm Views when it is triggered.

  4. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Functions
  • Alarms Overview
  • Configuring the Audibility of an Alarm
  • Configuring the Audibility of an Alarm in Reset State
  • Configuring a Custom Audible Alarm Alert
  • Turning off a Visual and Audible Alert
  • Create Alarm Wizard – Presentation Page