Configuring the Limits of an Alarm
You configure the limits of an alarm to adjust when an alam triggers or resets.
To configure the limits of an alarm
In WorkStation, in the
System Tree
pane, select the alarm you want to configure.
Click the
Alarm Trigger
tab.
In the
Alarm limit
boxes, enter the limits for the alarm.
action_zoom_plus_stroke
In the
Changes have been made
dialog box, click
Yes
to save the changes.
Alarms Overview
Create Out of Range Alarm Wizard – Alarm Trigger Page
Create Change of State Alarm Wizard – Alarm Trigger Page
Create Multistate Alarm Wizard – Alarm Trigger Page
Create Matching Text String Alarm Wizard – Alarm Trigger Page
Create Out of Reference Range Alarm Wizard – Alarm Trigger Page
Create Sum Alarm Wizard – Alarm Trigger Page
Create Enumeration Alarm Wizard – Alarm Trigger Page
Create Variable Status Alarm Wizard – Alarm Trigger Page