earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 警报
产品版本: 1.8
2016/10/13

Configuring the Priority of an Alarm

You configure the priority level of the different alarm states ​to ​meet the unique needs of your site.

To configure the priority of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. Click the Presentation tab.

  3. ​Under Priorities , select the Same priority check box to enter the same priority.

     
    action_zoom_plus_stroke
  4. In the Priorities boxes, enter the priority for each alarm state.

  5. In the Changes have been made dialog box, click Yes to save the changes.

  • Create Alarm Wizard – Presentation Page
  • Priority