earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Tendances
Version produit : 2.0, 2.1, 3.0, 3.1
15/07/2019

Configuration du fuseau horaire de la courbe de tendance

Vous affichez l'heure des enregistrements en heure locale, heure serveur ou heure d'un fuseau horaire prédéfini. En modifiant les préférences de fuseau horaire, vous facilitez l'interprétation de l'horodatage.

Afficher plus
action_close

​In a trend chart, you can present the records of a trend log in different time zones: local time or a predefined time zone.

​A time zone is a region on the earth that has a uniform standard time, usually referred to as the local time. Local time is the UTC time plus the current time zone offset for the considered location. Some time zones also have an offset called DST added during the summer period. The DST offset is typically +1 hour.

Before you set the time zone for a trend chart, you should consider these settings:

  • Computer clock settings​

  • Regional settings

A computer clock displays time that has been set manually or by synchronizing to a time server. The computer clock time shows local time. Regional time displays the time of the selected location. Asynchronous computer clock time and regional time are not uncommon and can cause, for example, unexpected time discrepancies between time stamps on received values and the computer clock time.

​To adjust the SmartX server time, time zone, and DST, you have to access the SmartX server through a WorkStation.

Local Time

A trend chart presented in Local time displays trend logs with time stamps adjusted for the client computer time zone.

The client computer does not consider the local time of the EcoStruxure BMS server where the variable is logged. The same variable logged on EcoStruxure BMS servers in different time zones is displayed with matching time stamps for corresponding values.

 
action_zoom_plus_stroke Local time zone, schematic
Figure : Local time zone, schematic

Predefined Time Zone

A trend chart presented in a predefined time zone displays trend logs in the time of the selected time zone regardless of where the EcoStruxure BMS server is located.

The same variable logged on EcoStruxure BMS servers in different time zones are displayed with adjusted time stamps for corresponding values. Use predefined time zone when you need to compare trend logs on EcoStruxure BMS servers located in different time zones.​

 
action_zoom_plus_stroke Predefined time zone, schematic
Figure : Predefined time zone, schematic

Pour configurer le mode Fuseau horaire de la courbe de tendance
  1. Dans WorkStation, dans le volet arborescence du système , sélectionnez la courbe de tendance que vous souhaitez configurer.

  2. Dans la vue Courbe de tendance, cliquez sur le bouton Ouvrir les paramètres de courbe de tendance

     
    action_zoom_plus_stroke
    dans la barre d'outils.

  3. Dans la boîte de dialogue Paramètres de la courbe de tendance , dans le champ Fuseau horaire , sélectionnez un fuseau horaire à appliquer à l'horodatage de la courbe de tendance dans :

    • Sélectionnez l' heure locale pour afficher l'horodatage en temps réel du point de vue du client.

    • Sélectionnez un fuseau horaire prédéfini pour afficher l'horodatage en temps réel du point de vue du fuseau horaire sélectionné.

  4. Cliquez sur OK .

L'axe X est maintenant défini en fonction du fuseau horaire sélectionné.

  • Time Zone Modes in a Trend Chart
  • Icônes des événements de courbe de tendance