Productos AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 3.2, 3.3, 2022
20/07/2021

Configuring the X-Axis with a Relative Time Span

You set the trend chart time span of the x-axis relative to the series current end point time to automatically adapt the trend chart to display the current time and the latest records within the specific time span.

Mostrar más
action_close

The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.

 
action_zoom_plus_stroke Absolute time span and relative time span, schematic
Figura: Absolute time span and relative time span, schematic

The y-axis refers to the measurement unit that the variable represents. The scale of the y-axis can be set manually or by auto scale. You can configure the trend chart to present series on one y-axis or two y-axes, one to the left and one to the right. Use two y-axes to present series with different ranges in the same trend chart.

 
action_zoom_plus_stroke One y-axis and two y-axes, schematic
Figura: One y-axis and two y-axes, schematic

To make reading easier, grid lines can be shown in the trend chart. Grid lines can be shown in both the x- and y-direction, independent of each other.

 
action_zoom_plus_stroke Grid lines, schematic
Figura: Grid lines, schematic

To configure the x-axis with a relative time span
  1. In WorkStation, in the System Tree pane, select the trend chart you want to configure.

  2. In the trend chart view, on the toolbar, click Open trend chart settings button

     
    action_zoom_plus_stroke
    .

  3. In the Trend chart settings dialog box, in the Time mode box, select Relative (to current time) .

  4. In the Time span box, type the length of the x-axis to display before the current time .

  5. Click OK .

The x-axis is now configured with a relative time span.

  • Trend Chart Axes
  • Configuring the X-Axis with an Absolute Time Span
  • Trend Chart Event Icons
  • Trend Chart Settings Dialog Box – Axes Tab
  • Trend Chart Does Not Show Trend Log Series