earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
12/10/2017

Control Panel – Backup and Archiving

Use the Backup and Archiving options on the Control Panel to create new backup rules, diagnose backup or restore issues, and view the current status of a SmartStruxure server.

 
action_zoom_plus_stroke Control Panel – Backup and archiving
Figura: Control Panel – Backup and archiving

Tabla: Control Panel – Backup and Archiving

Component

Description

Backup Rules

Click to open the Backup Rules view where you manage backup rules. You can also modify the backup schedule associated with the backup rule. Para obtener más información, consulte Backup Rules View .

Backup Sets

Click to open the Backup Sets view where you manage backup sets. Para obtener más información, consulte Backup Sets View .

Backup and Restore Manager

Click to open the Backup and Restore Manager where you view current backup and restore statuses and configure Purge settings for an Enterprise Server. Para obtener más información, consulte Backup and Restore Manager on the Enterprise Server .

Archiving

Click to open the Archive Settings where you enable the archiving function, set delay, and select the format of the archive file. Para obtener más información, consulte Archiving Settings Properties – Basic Tab .

  • Backup and Restore Overview
  • Backup Rules View
  • Backup Sets View
  • Backup and Restore Manager on the Enterprise Server
  • Archiving Settings Properties – Basic Tab