earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 3.2, 3.3, 2022
2020-10-15

Control Panel – Backup and Archiving

Use the Backup and Archiving options on the Control Panel to create new backup rules, diagnose backup or restore issues, and view the current status of an EcoStruxure BMS server.

 
action_zoom_plus_stroke Control Panel – Backup and archiving
Figur: Control Panel – Backup and archiving

Tabell: Control Panel – Backup and Archiving

Component

Description

Backup Rules

Click to open the Backup Rules view where you manage backup rules. You can also modify the backup schedule associated with the backup rule. Mer information finns i Backup Rules View .

Backup Sets

Click to open the Backup Sets view where you manage backup sets. Mer information finns i Backup Sets View .

Backup and Restore Manager

Click to open the Backup and Restore Manager where you view current backup and restore statuses and configure Purge settings for an Enterprise Server. Mer information finns i Backup and Restore Manager on the Enterprise Server .

Archiving

Click to open the Archive Settings where you enable the archiving function, set delay, and select the format of the archive file. Mer information finns i Archiving Settings Properties – Basic Tab .

  • Backup and Restore Overview
  • Backup Rules View
  • Backup Sets View
  • Backup and Restore Manager on the Enterprise Server
  • Archiving Settings Properties – Basic Tab