earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
5
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2019/6/26

Saving a SmartX Server Backup Set to Another Location

You save a backup set from a SmartX server to another location so you can store the backup set on, for example, a network drive or a USB memory.

To save a SmartX server backup set to another location
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the EcoStruxure BMS server.

  3. Click Backup Sets .

  4. In the List View , open the Local folder for a SmartX server or the AS Archives folder for an Enterprise Server.

  5. If connected to the Enterprise Server, open the SmartX server folder that contains the backup set.

  6. Select the backup set that you want to save to a different location.

  7. On the Actions menu, click Save To .

  8. In the Save As dialog box, enter a storage location and click Save .

  9. Click Close .

  • Backup Sets
  • Control Panel Tab
  • Backup Sets View
  • No Restore Files Display After Backup
  • Importing a Backup Set to SmartX Server
  • Renamed SmartX Server Makes Backup Sets Unavailable
  • Cannot Save a Backup File using WorkStation