earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018/6/26

Saving an Enterprise Server or Enterprise Central Backup Set to Another Location

You save a backup set from an Enterprise Server or Enterprise Central to another location, for example, a network drive or a USB memory.

显示更多
action_close

EcoStruxure BMS servers store backup sets in their local directories. By design, the average user may not easily locate these backup directories using a Windows-based file system. For convenience, you can save backup sets stored on EcoStruxure BMS servers to WorkStation. After saving the backup set, you can also copy the file to another backup storage location.

Saving a backup set to a storage location is a two-step process: saving the backup set and then relocating the file to another location. First, you save the backup set to WorkStation. Second, you copy the backup set from WorkStation to another storage location on your network, such as a USB drive.

 
action_zoom_plus_stroke Copy backup set from an automation server to a network drive
图: Copy backup set from an automation server to a network drive
Uniquely Named Storage Directory

To save time, you can create a uniquely named directory in which to store your saved backup sets for a particular EcoStruxure BMS server. This unique folder name can help you identify a particular Enterprise Server or automation server backup set, such as AS-1 Final Configuration Backup. Using this method, you can easily locate the backup set on your network.

Backup Set Renaming

Scheduled backup sets have a unique file name and extension based on the date stamp and server name. However, you can rename the backup set, if necessary. 有关更多信息,请参阅 Scheduled Backups .

Backup Set Removal

You can remove backups sets in two ways:

To save an Enterprise Server or Enterprise Central backup set to another location
  1. On the Tools menu, select Control Panel .

  2. On the Control Panel toolbar, select the Enterprise Server or Enterprise Central.

  3. Click Backup Sets .

  4. In the List View , open the Local folder.

  5. Select the Enterprise Server backup set that you want to save to a different location.

  6. On the Actions menu, click Save to .

  7. In the Save As dialog box, enter a storage location and click Save .

  8. Click Close .

  • Backup Sets View
  • Backup Set Storage and Protection