功能: 警报
产品版本: 1.8
2016/10/13

Creating a Category

You create a category to group alarms so that alarms are more easily identified.

显示更多
action_close

​You can group together alarms in categories to simplify the identification of the alarm. When the alarm is triggered, the category name is displayed together with the alarm in the Alarms pane, Events pane, Alarm Views, and Event Views.

For example, you create a category called “Building A” and add all alarms represented in the building to this category. Another example could be that you create a category called “Door alarm” and select this category for every door alarm in the system.

To create a category
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Categories .

  4. Click the Categories tab, and then click the Add category button

     
    action_zoom_plus_stroke
    .

  5. In the Name box, type the name of the new category.

     
    action_zoom_plus_stroke
  6. In the Description box, type a description for the category.

  7. Click OK .

  8. On the File menu, click Save .

  • Configuring the Category of an Alarm
  • Alarm Control Panel – Categories View
  • Categories