earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Creating a Category

You create a category to group alarms so that alarms are more easily identified.

显示更多
action_close

​You can group together alarms in categories to simplify the identification of the alarm. When the alarm is triggered, the category name is displayed together with the alarm in the Alarms pane, Events pane, Alarm Views, and Event Views. Each alarm can belong to two categories.

Example 1:

You create a category called 'Building A' and add all alarms represented in the building to this category. Another example could be that you create a category called “Door alarm” and select this category for every door alarm in the system.

Example 2:

You create a Category 2 called 'Alarms to Enterprise Central' on an Enterprise Server. You then create an alarm decoration rule and configure the Category 2 of the alarm decoration rule to 'Alarms to Enterprise Central'. On Enterprise Central, you configure an alarm filter to show alarms where the Category 2 property is 'Alarms to Enterprise Central'.

有关更多信息,请参阅 Configure Alarm Filters on Enterprise Central Workflow .

To create a category
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Categories .

  4. In the Categories tab, click the Add category button

     
    action_zoom_plus_stroke
    .

  5. In the Add Category dialog box, in the Name box, type the name of the new category.

  6. In the Description box, type a description for the category.

  7. Click OK .

  8. On the File menu, click Save .

  • Configuring the Category of an Alarm
  • Alarm Control Panel – Categories View
  • Alarm Categories