earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/3

Creating a Filtered Event View

​​You create a new filtered Event View to monitor and handle events. By adding an event filter you only display events that you are interested in.

显示更多
action_close

You can style certain events to bring out those that are of more interest than other events listed in the Events pane and Event Views. To style a specific event, you first have to create a condition that is associated with the events you want to style. An event can be styled with a unique background color, font, and font color.

For example, you can style all events where an alarm is acknowledged. To separate this event from others you configure, change the background color to dark green and the font color to white. All other events have the default style which is a white background and black font color.

If an event fulfills the condition criteria in more than one of the configured event criteria, it is the event style with highest priority in the Events View Style dialog box that is applied to the event.

Events styling does not apply to WebStation and does not affect the events in WebStation.

Event View standard filter and layout

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

有关更多信息,请参阅 Alarm View and Event View Standard Filter and Layout .

To create a filtered Event View
  1. ​In WorkStation, in the System Tree pane, ​select the folder or EcoStruxure BMS server where you want to create the event.

  2. On the File menu, point to New and then click View .

  3. In the Create Object wizard, in the object type list, click Event View .

  4. In the Name box, type a name for the Event View.

  5. In the Description box, type a description for the Event View.

  6. Click Create .

  7. In the System Tree pane, select the Event View that you created.

  8. On the Actions menu, click Edit standard Event View filter .

  9. In the Select Conditions dialog box, click the Add Condition button

     
    action_zoom_plus_stroke
    and select a condition.

  10. In the Add/Remove Conditions dialog box, select a condition and then click OK .

  11. In the Select Conditions dialog box, enter the settings of the condition.

    提示:

    ​You can add several event view conditions to specify when to write to the Event View.

  12. ​Click the Add row button

     
    action_zoom_plus_stroke
    to add another condition of the same type.

  13. Click OK .

  • Events Pane and Event View Customization
  • Event Filter Conditions
  • Styling a Certain Event in the Events Pane or Event View
  • Alarm View and Event View Standard Filter and Layout
  • Favorites
  • Event Is Not Displayed in the Events Pane and Event View
  • Events Pane and Event View Toolbar
  • Event View Properties
  • Select Conditions Dialog Box
  • Add/Remove Conditions Dialog Box