Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Calendriers
Version produit : 2024, 7.0
03/12/2024

Creating a Multistate Schedule

You create a multistate schedule to control the state of a multistate value.

Afficher plus
action_close

A multistate schedule controls a device that has output states based on integers or positive whole numbers including zero.

For example, you can create a multistate weekly schedule that is bound to a multistate value to control an air handler unit in an office building. To regulate the air circulation Monday through Friday from 08:00 to 17:00, you can set the value to 2 (occupied) when the schedule is active and 1 (unoccupied) when the schedule is inactive.

 
action_zoom_plus_stroke Multistate Schedule
Figure : Multistate Schedule

To create a multistate schedule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server or the folder where you want to create the schedule.

  2. On the File menu, point to New and then click Schedule .

  3. In the Create Object wizard, in the object type list, select Multistate Schedule .

  4. In the Name box, type a name for the schedule.

  5. In the Description box, type a description for the schedule.

  6. Click Create .

Now you can add events to the multistate schedule and bind it to a multistate value.

  • Schedule Types
  • Multistate Schedules
  • Create Object Dialog – Naming the Object Page
  • Binding a Multistate Value to a Multistate Schedule
  • Adding a Weekly Event
  • Adding a Calendar Exception Event
  • Adding a Date Exception Event
  • Adding a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Create Object Dialog – Naming the Object Page