earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2.0, 2.1, 3.0, 3.1
2018/12/27

Creating a Panel

You create panels to customize framing in a workspace. For example, panels can display particular graphics or menus that are visible as frames in the WorkStation Work area.

显示更多
action_close

You use a panel to combine different viewable windows, for example, a graphic, trend chart, report, or another panel into a seamless view. A panel consists of one or several panes and one work area.  The panel is available through the System Tree pane and opens as a window in the work area of the current workspace.

 
action_zoom_plus_stroke Example of panel components
图: Example of panel components

In the procedure when creating a panel, you link existing objects to the panes or workspace that is added within the panel. Therefore, you have to first create the object, for example a trend chart, before you add or rather link in the object into the panel. You can define whether to show or hide a pane's toolbar.

注释:
  • A panel cannot contain a System Tree pane.

  • A maximum of six levels of panels are allowed in a single pane. However, the recommendation for a good user experience is to only use three levels.

In a graphic or in the content of a pane or work area, you can create links that point to a panel. ​By using panels, you streamline the information you want to present to the user. For example, you have a graphic that represents a room. In the room illustration, you add a fan symbol to which you link a panel containing panes and a work area that displays the current room airflow and temperature.

You can use a navigation pane to build a customized structure for navigation. The navigation pane can be used in a panel. 有关更多信息,请参阅 Customized Navigation .

To create a panel
  1. In WorkStation, in the System Tree pane, select in the folder where you want to create the panel.

  2. On the File menu, point to New and then click Panel .

  3. In the Create Object wizard, in the Name box, type a name for the panel.

  4. In the Description box, type a description for the panel.

  5. Click Next .

  6. In the Panel Configuration page, click the Add button

     
    action_zoom_plus_stroke
    to add an object to the panel. you add an object to the panel.

  7. In the Create Object wizard, in the object type list, select the type of panel component you want to add.

  8. In the Name box, type a name for the component.

  9. In the Description box, type a description for the panel component.

  10. Click Next .

  11. In the Pane Configuration page, in the Show toolbar box, select Yes to show the toolbar of the component.

  12. In the Default dock position box, select where the component should be located.

  13. In the Default visibility box, select Visible to show the component in the panel by default.

  14. In the Display name box, type the name to be displayed on the pane.

  15. In the Initial path box, enter the path to the object you are adding to the panel.

  16. Click Create .

  17. In the Work area initial path box, enter the initial object that displays when viewing this panel.

  18. In the Show toolbars box, select Yes to display the toolbar for the object listed in the initial path.

  19. Click Create .

  • Panel Components
  • Create Object Wizard – Naming the Object Page
  • Panel Wizard – Panel Configuration Page
  • Editing a Panel