You create a trend chart that monitories a variable in real-time, for example, to access and check the current status of the variable.
In WorkStation, in the System Tree pane, select the folder or SmartStruxure server where you want to create the trend chart.
On the File menu, point to New and then click Trend .
Select Trend Chart .
In the Name box, type a name for the trend chart.
In the Description box, type a description.
Click Next .
In the Time mode box, select Absolute to manually specify the x-axis start and end point.
In the Start time box, type the absolute start time (the leftmost point of the x axis).
In the End time box, type the absolute end time (the rightmost point of the x axis).
In the Auto scale left y-axis box, select True so the y-axis adapts itself to displayed series.
Click the Add
Select Real Time Trend Series .
In the Name box, type a name for the series.
In the Description box, type a description.
Click Next .
In the Display variable box, enter the variable you want to display in the trend chart.
In the Weight box, select the weight of the series.
In the Show markers box, select True to display a marker for each recorded.
Click Create .
In the Configure real-time trend series dialog box, click Create .
The real-time trend series trend chart is created in the selected folder.