earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: WebStation
Функции: Управление пользователями
Версия продукта: 2024, 7.0
03.12.2024

Creating a User Account

You create a user account when you want a person to have access to the EcoStruxure BMS.

Показать больше
action_close

Using WebStation, you can create and administer user accounts.

You can also add a new user account to an already existing user group in the system. You can force users to change their password the next time they log on. Unused accounts can be disabled and saved for further use or they can be deleted from the system.

To create a user account
  1. In WebStation, click Open workspace menu .

  2. Click System.

  3. Click Domains .

  4. Click the Domain where you want to create the user.

  5. Click Users .

  6. In the Users pane, click Add .

  7. In the User name box, type the user name.

  8. In the Password box, type the password.

  9. In the First name box, type the first name.

  10. In the Middle name box, type the middle name.

  11. In the Last name box, type the last name.

  12. In the Home email box, type the home email address.

  13. In the Work email box, type the work email address.

  14. Click the Access tab

  15. In the Disable field, select True to disable the account.

  16. In the Force password change field, select True to force the user to change the password the next time the user logs on.

  17. In the Expiration box, enter the expiration date for the user account.

  18. In the Member of box, select the user groups you want the user to be a member of.

  19. Click the Appearance tab.

  20. In the Language list, select the language.

  21. In the Date, time and number format list, select the date, time and number format.

  22. In the System of measurement list, select the system of measurement.

  23. In the Relative Time field, enter how to handle relative time.

  24. In the Dark Mode field, enter how to handle dark mode.

  25. In the Size Mode field, enter the size of fonts and icons.

  26. In the Workspace Layout field, select the workspace.

  27. Click Save .

  • Create and Administer User Accounts in WebStation
  • Theme Settings
  • Password Policy
  • Forcing Users to Change Their Passwords
  • Disabling a User Account
  • Deleting a User Account
  • User Management Dialog Box – Profile Tab