earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Localización
Versión del producto: 2023, 2024, 7.0
01/12/2024

Date and Time Properties – Time Tab

Use the Time tab to configure the network time server addresses or establish a lead and shadow relationship on EcoStruxure BMS servers.

 
action_zoom_plus_stroke Time tab
Figura: Time tab

Tabla: Time Tab

Component

Description

Use external NTP server

Select Enabled to define the primary and secondary NTP server addresses for connected shadow automation server.

NTP Server 1

​Type the address to the primary time server to which the shadow automation server date and time object synchronizes its clock.

NTP Server 2

Type the address to the secondary time server to which the shadow automation servers' date and time object synchronizes its clock.

Lead object

​Enter the object that acts as the lead for this object.

Primary time server Key Id

Type the ID of the authentication key for the primary time server.

Secondary time server Key Id

Type the ID of the authentication key for the secondary time server.

Password

Type the password for the primary time server.

Confirm Password

Type the password for the primary time server again.

Password

Type the password for the secondary time server.

Confirm Password

Type the password for the secondary time server again.

Authenticate Network Time Synchronization

Select if you want to use authenticated network time synchronizing.

  • Network Time
  • Network Time Settings Synchronization
  • Date & Time View
  • Date and Time Properties – Basic Tab