earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Conceito

Conceito


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmes
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Deadband

​Deadband is an area of the alarm range where no reset action occurs. The purpose of the deadband is to prevent unintentional activation-deactivation cycles.

For example, an out of range alarm has an upper limit of 10 and the deadband is 2. The monitored variable must be equal to or fall below 8 (10-2) before the triggered alarm is reset.

 
action_zoom_plus_stroke The monitored variable has to reach the limit of the deadband before the alarm is reset.
Imagem: The monitored variable has to reach the limit of the deadband before the alarm is reset.

Deadband can be set for out of range alarms and out of reference range alarms.

  • Alarms Overview
  • Alarm Functions
  • Configuring the Limits of an Alarm