earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Deleting a Backup Rule

You delete a backup rule to remove the rule from the SmartStruxure server.

Show More
action_close

In Building Operation, scheduled backups are managed by backup rules, which are conditions that govern behavior. Similar to a scheduled task, a backup rule performs a backup on a SmartStruxure server using three pieces of data: when the backup occurs, what type of data will be backed up, and a comment describing the purpose of the backup.

Building Operation automatically backs up all data on a SmartStruxure server every Sunday at 01:00. However, you can change the backup rule settings. For example, you can change the type of data you want to back up.

You can create your own backup rules to complete different tasks on different SmartStruxure servers. For example, you can create a backup rule that backs up all data on the Enterprise Server twice a day rather than once a week based on the default setting. In addition, you can set up another backup rule for one SmartStruxure server, which acts as the lead, to manage a recurring backup for a group of SmartStruxure servers. For more information, see Backup Rules View .

To delete a backup rule
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Backup Rules .

  4. Select the backup rule and then click the Remove backup rule button

     
    action_zoom_plus_stroke
    .

     
    action_zoom_plus_stroke
  5. Click Yes to delete the backup rule from the SmartStruxure server.

     
    action_zoom_plus_stroke
  6. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Backup Rules
  • Scheduled Backups
  • Creating a Backup Rule
  • Backup Rules View