earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1
25/10/2018

Deleting a Backup Rule

You delete a backup rule to remove the rule from the EcoStruxure BMS server.

Afficher plus
action_close

The EcoStruxure Building Operation scheduled backups are managed by backup rules, which are conditions that govern behavior. Similar to a scheduled task, a backup rule performs a backup on an EcoStruxure BMS server using three pieces of data: when the backup occurs, what type of data will be backed up, and a comment describing the purpose of the backup.

The EcoStruxure Building Operation software automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. However, you can change the backup rule settings. For example, you can change the type of data you want to back up.

You can create your own backup rules to complete different tasks on different EcoStruxure BMS servers. For example, you can create a backup rule that backs up all data on the Enterprise Server twice a day rather than once a week based on the default setting. In addition, you can set up another backup rule for one EcoStruxure BMS server, which acts as the lead, to manage a recurring backup for a group of EcoStruxure BMS servers. Pour plus d'informations, voir Backup Rules View .

To delete a backup rule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup Rules .

  4. In the Backup rules view, select the backup rule and then click the Remove backup rule button

     
    action_zoom_plus_stroke
    .

  5. Click Yes to delete the backup rule from the EcoStruxure BMS server.

  6. On the File menu, click Save .

  • Backup Rules
  • Scheduled Backups
  • Control Panel Tab
  • Creating a Backup Rule
  • Backup Rules View