earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1
12/19/2019

Alarm Handling Issues

When an alarm is triggered it appears in the alarm list. You can acknowledge, disable, or hide alarms in the alarm list. An acknowledged alarm disappears from the alarm list when it has been reset to normal state.

When the alarm database gets corrupted after an EcoStruxure BMS server crash, all alarms are re-evaluated. The alarms that are still active are resent to the alarm database. However, the information that an alarm has been acknowledged, disabled, or hidden is lost, and you have to repeat operations you performed on the alarm before the data loss.

When an alarm has been triggered and reset to normal state without having been acknowledged, the alarm remains in the alarm list until it is acknowledged. If the alarm is lost, an alarm refresh does not make the alarm reappear in the alarm list. The alarm is reset and has no alarm state to send.

Most system information alarms are only messages. These alarms cannot be in an alarm state, thus, an alarm refresh does not make the system information alarms reappear in the alarm list.

  • Alarm States
  • Alarms Pane and Alarm View
  • Enterprise Server System Upgrade Workflow