earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 警报
产品版本: 2023
2022/12/16

Alarm Handling Issues

When an alarm is triggered it appears in the alarm list. You can acknowledge, disable, or hide alarms in the alarm list. An acknowledged alarm disappears from the alarm list when it has been reset to normal state.

When the alarm database gets corrupted after an EcoStruxure BMS server crash, all alarms are re-evaluated. The alarms that are still active are resent to the alarm database. However, the information that an alarm has been acknowledged, disabled, or hidden is lost, and you have to repeat operations you performed on the alarm before the data loss.

When an alarm has been triggered and reset to normal state without having been acknowledged, the alarm remains in the alarm list until it is acknowledged. If the alarm is lost, an alarm refresh does not make the alarm reappear in the alarm list. The alarm is reset and has no alarm state to send.

Most system information alarms are only messages. These alarms cannot be in an alarm state, thus, an alarm refresh does not make the system information alarms reappear in the alarm list.

  • Alarm States
  • 报警窗格和报警视图
  • Enterprise Server System Upgrade Workflow
  • Checking the Integrity of an Alarm