earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool, WebStation
Funktionaliteter: Tidsscheman
Produktversion: 3.2, 3.3, 2022
2021-07-20

Digital Schedules

A digital schedule controls a device that has an on output state and an off output state.

For example, you can create a digital weekly schedule that is bound to a digital output, such as a light switch. To turn on the lights Monday through Friday from 08:00 to 17:00, you can set the value to On when the schedule is active and Off when the schedule is inactive.

 
action_zoom_plus_stroke Digital Schedule
Figur: Digital Schedule
  • Schedule Types
  • Creating a Digital Schedule
  • Modifying a Schedule Using the Text View
  • Modifying a Schedule Using the Graphic View