earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Como

Como


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmes
Versão do produto: 3.2, 3.3, 2022
21-02-2023

Displaying an Alarm View when an Alarm is Triggered

You configure the built-in Alarm pane to automatically open an Alarm View dialog box in a new window when an alarm is triggered.

To display an Alarm View when an alarm is triggered
  1. In WorkStation, in the built-in Alarms pane, right-click anywhere to display the context menu.

  2. Point to Alarm View settings and then click Display Alarm View on alarm .

  • Creating a Filtered Alarm View
  • Alarms Pane and Alarm View Customization
  • Alarm View Properties
  • Menu de contexto de painel de alarmes - submenu de definições de vista de alarme