earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Сигналы тревоги
Версия продукта: 2024, 7.0
03.12.2024

Displaying an Alarm View when an Alarm is Triggered

You configure the built-in Alarm pane to automatically open an Alarm View dialog box in a new window when an alarm is triggered.

To display an Alarm View when an alarm is triggered
  1. In WorkStation, in the built-in Alarms pane, right-click anywhere to display the context menu.

  2. Point to Alarm View settings and then click Display Alarm View on alarm .

  • Creating a Filtered Alarm View
  • Alarms Pane and Alarm View Customization
  • Alarm View Properties
  • Alarms Pane Context Menu - Alarm View Settings Submenu