earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Server, Virtual Project Servers
Functionalities: Trends
Product version: 1.8
10/13/2016

Displaying Meter Change History

You view, through a trend log list, all meter change events that are registered by the meter trend log.

Note:
  • The meter change history is only applicable for the meter trend log.

Show More
action_close

​The meter trend log is a variable triggered trend log with extra functionality to seamlessly handle consumption calculations independent of meter rollover or meter exchange.

For more information, see Variable Triggered Trend Logs .

You create and configure meter trend logs using WorkStation.

For example, in the figure below, the meter trend log records a meter the 1st of every month. In the middle of February the meter rolls over to 00000. A chart with meter consumption calculation prints the consumption every month.

 
action_zoom_plus_stroke Meter trend log
Figure: Meter trend log

When physically replacing an old meter with a new one, you have to configure the meter trend log by adding the settings of the old meter and new meter in the Manage replacement of meter dialog box in WorkStation. These settings are the foundation to handle a meter rollover or calculating consumption though meter replacement. For more information, see Manage Replacement of Meter Dialog Box .

 
action_zoom_plus_stroke Manage replacement of meter dialog box where you enter the values of the new and old meter.
Figure: Manage replacement of meter dialog box where you enter the values of the new and old meter.
Note:
  • In order for a meter rollover to be managed correctly in the meter trend log and to ensure logging starts at the correct energy reading value, you enter previous meter and new meter information in the Manage replacement of meter dialog box. For more information, see Managing Replacement of a Meter .

To display meter change history
  1. In WorkStation, in the System Tree pane, select the trend log list that is connected to a meter trend log.

  2. On the Trend Log List toolbar, click the Show list of meter change events button

     
    action_zoom_plus_stroke
    .

     
    action_zoom_plus_stroke
  3. Click Close .

It is important that all meter changes are registered in the Manage replacement of meter dialog box.

  • Meter Trend Logs
  • Meter Change History Dialog Box
  • Managing Replacement of a Meter