earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Trends
Product version: 2.0, 2.1, 3.0, 3.1
9/4/2018

Displaying Meter Change History

You view, through a trend log list, all meter change events that are registered by the meter trend log.

Note:
  • The meter change history is only applicable for the meter trend log.

Show More
action_close

​The meter function adds meter properties to any trend log type to seamlessly handle consumption calculations independent of meter rollover or meter exchange.

You create and configure the meter function in trend logs using WorkStation.

For example, in the figure below, the meter function in the trend log records a meter the 1st of every month. In the middle of February, the meter rolls over to 00000. A chart with meter consumption calculation prints the consumption every month.

 
action_zoom_plus_stroke Meter trend log
Figure: Meter trend log

The calculation function supports negative meter consumption values, which can be used to handle cases where you need to subtract consumption, for example, when energy is produced on site.

When physically replacing an old meter with a new one, you have to configure the meter function of the trend log by adding the configuration and values of both the old and the new meter. These configurations and values are the foundation when handling a meter rollover or calculating consumption though meter replacement. For more information, see Managing Meter Replacement .

 
action_zoom_plus_stroke Manage replacement of meter dialog box where you enter the values of both the old and the new meter
Figure: Manage replacement of meter dialog box where you enter the values of both the old and the new meter
Note:
  • In order for a meter rollover to be managed correctly in the meter trend log and to ensure logging starts at the correct energy reading value, you enter previous meter and new meter information in the Manage replacement of meter dialog box. For more information, see Managing Meter Replacement .

To display meter change history
  1. In WorkStation, in the System Tree pane, select the trend log list that is connected to a meter trend log.

  2. On the Trend Log List toolbar, click the Show list of meter change events button

     
    action_zoom_plus_stroke
    .

  3. Click Close .

It is important that all meter changes are registered in the Manage replacement of meter dialog box.

  • Meter Function
  • Meter Change History Dialog Box
  • Managing Meter Replacement