earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: WorkStation
Функции: Тренды
Версия продукта: 2024, 7.0
03.12.2024

Displaying or Hiding Events in a Trend Log List

You hide or display events in a trend log list to make the reading easier. Events that have a value or comment cannot be hidden and are always displayed. For example, as a Record was added, or as a Record was commented.

Показать больше
action_close

A trend log list displays all values in the trend log in a list.

You can create a trend log list directly from a trend log and refresh the values.

You can manually add records to a trend log list for any type of trend log.

Trend Log List Display

A trend log list can be displayed in a number of ways.

Более подробную информацию см. Trend Log List Display .

Export of Trend Log Lists and Records

Trend log lists and records can be exported in two different formats:

  • CSV

  • XML

Более подробную информацию см. Export of Trend Log Lists and Records .

 
action_zoom_plus_stroke Trend log list
Рисунок: Trend log list

To display or hide events in a trend log list
  1. In WorkStation, in the System Tree pane, select the trend log list you want to display.

  2. On the Trend Log List toolbar, click the Events button

     
    action_zoom_plus_stroke
    .

Events are now displayed in the trend log list. Repeat the procedure to hide the events.

  • How Trend Logs Work
  • Trend Log Lists in WorkStation
  • Refreshing a Trend Log List
  • Trend Log List Toolbar
  • Trend Log List Event Icons