Funkcje: Trendy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Displaying the Trend Log List Time Stamps with Fractions

You display the trend log list time stamps with fractions, to show the exact time stamp when the value was recorded.

Pokaż więcej
action_close

​The trend log list numerically displays the records of a trend log or an extended trend log. The records of the trend log can be processed by a calculation method before they are presented in the trend log list.

The trend log list can only display one trend log at a time and must be manually refreshed to display recently recorded values.

 
action_zoom_plus_stroke Trend log list, schematic
Rysunek: Trend log list, schematic

You can manually add records to a trend log list for any type of trend log.

Time Zone Modes in a Trend Log List

​In a trend log list, you can present the records of a trend log in different time zones: local time zone, EcoStruxure BMS server time zone, and UTC time zone.

Więcej informacji zawiera Time Zone Modes in a Trend Log List .

Calculation Methods

​Use a calculation method to process the records of the trend log before presenting them in a trend log list or a trend chart. The original records in the trend log are not affected by the calculation method. The calculation method is applied to the trend log records grouped by a specific time interval.

Więcej informacji zawiera Calculation Methods .

Period Timestamps in Trend Charts and Trend Log Lists

When a calculated value for a period is presented, the middle of the period is used as the timestamp.

Example:

The calculated value for the period 8:00-9:00 is stamped 8:30. If there is a value at 9:01, the next period is 9:00-10:00, which is stamped as 9:30. The full period may not have passed yet, but the value can be presented even if parts of the period are in the future.

Temporary Trend Log Lists

​To display a trend log without creating a new trend log list or trend chart, the trend log can be displayed in a temporary list or chart.

Więcej informacji zawiera Temporary Trend Log Lists .

Floating Point Values NaN, INF, and -INF

In the EcoStruxure Building Operation software, the floating point values “Not a Number”, positive infinity, or negative infinity may be displayed in the Basic property tab, in a trend log list, or a trend chart.

Więcej informacji zawiera Floating Point Values NaN, INF, and –INF .

To display time stamps with fractions
  1. In WorkStation, in the System Tree pane, select the trend log list you want to display its time stamps in fractions.

  2. On the Trend Log List toolbar, click the Show time stamps with fractions button

     
    action_zoom_plus_stroke
    .

The time stamps in the trend log list are now shown with hundredths. Repeat the procedure to hide the fractions.

  • Trend Log Lists
  • Configuring a Trend Log List
  • Trend Log List Toolbar
  • Trend Log List View