earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 2.0, 2.1, 3.0, 3.1
28/12/2018

Domain – Domain Members Tab

Use the Domain Members tab to add and remove EcoStruxure BMS servers to and from the domain.

 
action_zoom_plus_stroke Domain members tab
Figura: Domain members tab

Tabla: Domain Members Tab

Component

Description

Available Servers

List of all available EcoStruxure BMS servers.

Servers that are members of this Domain

List of all EcoStruxure BMS servers in the domain.

 
action_zoom_plus_stroke

Add All

Click to add all available EcoStruxure BMS servers to the domain.

 
action_zoom_plus_stroke

Add

Click to add an EcoStruxure BMS server to the domain.

 
action_zoom_plus_stroke

Remove

Click to remove an EcoStruxure BMS server from the domain.

 
action_zoom_plus_stroke

Remove All

Click to remove all EcoStruxure BMS servers from the domain.

  • Domains