earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Backup Rule Dialog Box

Use the Backup Rule dialog box to change the type of data contained in the backup. You can also add a comment to identify the content or purpose of the backup. In addition, you can enable or disable the backup rule.

 
action_zoom_plus_stroke Backup Rule dialog box
Figura: Backup Rule dialog box

Tabla: Backup Rule Dialog Box

Component

Description

Name

Displays the name of the backup rule.

Backup set description

Type a description up to 255 characters that helps to identify the type and contents of the scheduled backup.

Backup content

Select the type of data that you want to back up.

Lead rule

Enter a backup rule that can act as a lead backup rule.

Enabled

Select Yes to enable the backup rule.

  • Scheduled Backups
  • Date and Time Properties – Basic Tab