earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Programaciones
Versión del producto: 2023
21/05/2024

Cuadro de diálogo Editar entrada de calendario – Fecha calculada

Utilice el cuadro Editar entrada de calendario para crear una entrada de calendario para un evento de excepción recurrente.

 
action_zoom_plus_stroke Cuadro de diálogo Editar entrada de calendario – Fecha calculada
Figura: Cuadro de diálogo Editar entrada de calendario – Fecha calculada

Tabla: Cuadro de diálogo Editar entrada de calendario – Fecha calculada

Componente

Descripción

Nombre de la entrada

Type an entry name for the calendar entry.

Mes

Select a month for the exception event or Odd month , Even month , Any month .

Semana del mes

Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

  • First week – the first through the seventh day of the month. Be aware that it does not necessarily correspond to the first row of the calendar since it may include dates from both the first and second row of the calendar.

  • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

  • Last week – the last seven days of the month. It differs from the Fifth wee k .

Día de la semana

Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  • Eventos de calendario