earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funktionaliteter: Tidsscheman
Produktversion: 2024, 7.0
2024-12-03

Edit Calendar Entry Dialog Box – Calculated Date

Use the Edit Calendar Entry dialog box to create a calendar entry for a recurring exception event.

 
action_zoom_plus_stroke Edit Calendar Entry dialog box - calculated date
Figur: Edit Calendar Entry dialog box - calculated date

Tabell: Edit Calendar Entry Dialog Box – Calculated Date

Component

Description

Entry name

Type an entry name for the calendar entry.

Month

Select a month for the exception event or Odd month , Even month , Any month .

Week of month

Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

  • First week – the first through the seventh day of the month. Be aware that it does not necessarily correspond to the first row of the calendar since it may include dates from both the first and second row of the calendar.

  • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

  • Last week – the last seven days of the month. It differs from the Fifth wee k .

Day of week

Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  • Calendar Events
  • General Information Properties – Basic Tab
  • References Tab