earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
12/3/2024

Edit Checklist Dialog Box

Use the Edit Checklist dialog box to add, edit, or order the steps of a checklist.

 
action_zoom_plus_stroke Edit Checklist dialog box
Figure: Edit Checklist dialog box

Table: Edit Checklist Dialog Box

Button

Description

Name

Type the name of the checklist.

Description

Type a description of the checklist.

 
action_zoom_plus_stroke

Add step

Click to open the Add checklist step dialog box where you add a step to your checklist. For more information, see Add Checklist Step Dialog Box .

 
action_zoom_plus_stroke

Edit step

Click to open the Edit checklist step dialog box where you edit a checklist step. For more information, see Edit Checklist Step Dialog Box .

 
action_zoom_plus_stroke

Remove step

Click to remove the selected step from the checklist.

 
action_zoom_plus_stroke

Move step up

Click to move the selected step upwards in the list.

 
action_zoom_plus_stroke

Move step down

Click to move the selected step downwards in the list.

  • User Actions
  • Add Checklist Step Dialog Box
  • Alarm Control Panel – Checklists View
  • Control Panel
  • Checklists
  • Edit Checklist Step Dialog Box