Use the Edit menu for standard editing of objects.
Command |
Description |
Search |
Click to open Search. For more information, see Search Overview . |
Cancel |
Click to cancel the latest command. |
Refresh |
Click to refresh the selected object or workspace. |
Select all |
Click to select all objects. |
Deselect all |
Click to deselect all objects. |
Cut |
Click to cut the selected objects. The objects are placed on the clipboard. |
Copy |
Click to copy the selected objects. The objects are placed on the clipboard. |
Paste |
Click to paste a copied or cut object. |
Paste as shortcut |
Pastes a shortcut to a (copied) folder or object into the selected folder or SmartStruxure server root. |
Paste special |
Pastes with the all external references intact. For more information, see Copy, Paste, Duplicate, Move, Rename, and Delete . |
Duplicate |
Click to create a configurable number of copies of an object. For more information, see Copy, Paste, Duplicate, Move, Rename, and Delete . |
Move |
Click to move an object to another location. For more information, see Copy, Paste, Duplicate, Move, Rename, and Delete . |
Delete |
Click to open the Confirm delete dialog box where you delete the selected object. For more information, see Confirm Delete Dialog Box . |
Rename |
Click to rename the selected object. |
Create shortcut |
Creates a new shortcut to a selected folder or object into the same folder as the target. |