earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaccia dell'utente

Interfaccia dell'utente


Prodotti: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funzionalità: Funzionalità di base
Versione del prodotto: 3.2, 3.3, 2022
16/10/2020

Edit Menu

Use the Edit menu for standard editing of objects.

 
action_zoom_plus_stroke Edit menu
Figura: Edit menu

Tabella: Edit Menu

Command

Description

Cancel

​Click to cancel the latest command.

Refresh

​​Click to refresh the selected object or workspace.

Select all

Click to select all objects.

Deselect all

Click to deselect all objects.

Cut

​Click to cut the selected objects. The objects are placed on the clipboard.

Copy

​Click to copy the selected objects. The objects are placed on the clipboard.

Paste

​Click to paste a copied or cut object.

Paste as shortcut

Pastes a shortcut to a (copied) folder or object into the selected folder or EcoStruxure BMS server root.

Paste special

Pastes with the all external references intact. Per maggior informazioni, consulta Copy, Paste, Duplicate, Move, Rename, and Delete .

Duplicate

Pastes with the all external references intact. Per maggior informazioni, consulta Copy, Paste, Duplicate, Move, Rename, and Delete .

Move

Click to move an object to another location. Per maggior informazioni, consulta Copy, Paste, Duplicate, Move, Rename, and Delete .

Delete

​Click to open the Confirm delete dialog box where you delete the selected object. Per maggior informazioni, consulta Confirm Delete Dialog Box .

Rename

Click to rename the selected object.

Create shortcut

Creates a new shortcut to a selected folder or object into the same folder as the target.

  • Barra strumenti di WorkStation
  • Search Overview
  • Copy, Paste, Duplicate, Move, Rename, and Delete
  • Confirm Delete Dialog Box