earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 基本功能
产品版本: 1.8
2016/10/14

Edit Menu

Use the Edit menu for standard editing of objects.

 
action_zoom_plus_stroke Edit menu
图: Edit menu

表格: Edit Menu

Command

Description

Cancel

​Click to cancel the latest command.

Refresh

​​Click to refresh the selected object or workspace.

Select all

Click to select all objects.

Deselect all

Click to deselect all objects.

Cut

​Click to cut the selected objects. The objects are placed on the clipboard.

Copy

​Click to copy the selected objects. The objects are placed on the clipboard.

Paste

​Click to paste a copied or cut object.

Paste as shortcut

Pastes a shortcut to a (copied) folder or object into the selected folder or SmartStruxure server root.

Paste special

Paste with the all external references intact. 有关更多信息,请参阅 Move, Copy, Paste, Rename, and Delete .

Move

Click to move an object to another location. 有关更多信息,请参阅 Move, Copy, Paste, Rename, and Delete .

Delete

​Click to open the Confirm delete dialog box where you delete the selected object. 有关更多信息,请参阅 Confirm Delete Dialog Box .

Rename

Click to rename the selected object.

Create shortcut

Creates a new shortcut to a selected folder or object into the same folder as the target.

  • 工作站工具栏
  • Confirm Delete Dialog Box
  • Move, Copy, Paste, Rename, and Delete