earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Programaciones
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Edit Time Value Period Dialog Box

Use the Edit Time Value Period dialog box to modify weekly or exception events in the Advanced Schedule Editor.

 
action_zoom_plus_stroke Edit Time Value Period dialog box
Figura: Edit Time Value Period dialog box

Tabla: Edit Time Value Period Dialog Box

Component

Description

Value

Enter the value associated with the event.

Start Time

Click the up or down arrows to select the hours, minutes, and seconds for the start time. You can also type the time if you want.

End Time

Click the up or down arrows to select the hours, minutes, and seconds for the end time. You can also type the time if you want.

No End Time

Click the checkbox to have the event last all day.

  • Advanced Schedule Editor – Graphic View