earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/9/4

Editing a Backup Schedule

You edit a backup schedule, which is combined with a backup rule, to change the frequency of the backup. 

显示更多
action_close

The EcoStruxure Building Operation database includes a digital schedule that is combined with a default backup rule. Using this schedule and rule, the system automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. You can edit the schedule settings for this backup rule, but you cannot delete the schedule and select another.

有关更多信息,请参阅 Editing a Backup Schedule .

重要:

If the automatically scheduled backup occurs during a Daylight Savings Time transition, the backup will not occur. To prevent loss of data, change the scheduled backup to a time that does not conflict with your region's Daylight Savings Time transition.

 
action_zoom_plus_stroke Backup on a standalone SmartX server
图: Backup on a standalone SmartX server

You can create a custom backup rule and then modify its schedule. For example, you can create a backup rule that backs up all data on a SmartX server daily at 02:00.

有关更多信息,请参阅 Creating a Backup Rule .

To edit a backup schedule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup rules .

  4. In the Backup Rules view, in the Schedule column, click the schedule that you want to modify.

  5. Revise the schedule and then click the Save button

     
    action_zoom_plus_stroke
    .

  • Backup Schedules
  • Backup Rules View
  • 添加每周事件
  • 编辑每周事件
  • 添加日期例外事件
  • 编辑日期例外事件
  • 添加日期范围例外事件
  • 编辑日期范围例外事件
  • 添加计算的例外事件
  • 编辑计算的例外事件
  • 时间表编辑器 – 基本视图
  • Synchronizing EcoStruxure BMS Server Backups on a Network
  • Backup Rules View
  • Advanced Schedule Editor – Graphic View
  • Edit Time Value Period Dialog Box