earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Расписания
Версия продукта: 2024, 7.0
03.12.2024

Editing a Calculated Date Calendar Event

You edit a calculated date calendar to change the information about a calendar event.

To edit a calculated date calendar event
  1. In WorkStation, in the System Tree pane, select the calendar you want to edit.

  2. In Calendar Editor , select the calculated date calendar.

  3. Right-click the calculated date calendar.

  4. In the Edit Calendar Entry dialog box, edit the properties.

    Таблица: Edit Calendar Entry Dialog Box - Calculated date

    Component

    Description

    Entry name

    Type an entry name for the calendar entry.

    Month

    Select a month for the exception event or Odd month , Even month , Any month .

    Week of month

    Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

    • First week – the first through the seventh day of the month. Be aware that it does not necessarily correspond to the first row of the calendar since it may include dates from both the first and second row of the calendar.

    • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

    • Last week – the last seven days of the month. It differs from the Fifth wee k .

    Day of week

    Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  5. Click OK .

  • Edit Calendar Entry Dialog Box – Calculated Date
  • Calendar Editor Overview
  • General Information Properties – Basic Tab
  • References Tab