Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2022-07-12

Editing a Cause Note

You edit an existing cause note to change the name or the descriptions, or add the cause note to another cause note group.

To edit a cause note
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Cause notes .

  4. In the Cause notes view, select the cause note you want to edit .

  5. Click the Edit cause note button

     
    action_zoom_plus_stroke
    .

    Uwaga
    • To permanently remove a cause note from the cause notes list, click the Remove cause note button

       
      action_zoom_plus_stroke
      .

  6. In the Edit Cause Note dialog box, in the Name box, type a name for the cause note.

  7. In the Group name box, type a name to create a new group or select an existing group.

  8. In the Description box, type a description for the cause note.

  9. Click OK .

  10. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Cause Notes View
  • Creating a Cause Note
  • Adding a Cause Note to an Alarm
  • Adding a Cause Note to an Alarm in WebStation
  • Configuring Forced User Actions
  • Import and Export of Supporting Objects
  • Creating a Cause Note
  • Alarm Control Panel – Cause Notes View
  • Cause Notes