earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Расписания
Версия продукта: 2024, 7.0
03.12.2024

Editing a Date Range Calendar Event

You edit a date range calendar to change the information about a calendar event.

To edit a date range calendar event
  1. In WorkStation, in the System Tree pane, select the calendar you want to edit.

  2. In Calendar Editor , select the date range calendar.

  3. Right-click the date range calendar.

  4. In the Edit Calendar Entry dialog box, edit the properties.

    Таблица: Edit Calendar Entry Dialog Box - Date range

    Component

    Description

    Entry name

    Type an entry name for the calendar entry.

    Start year

    Select a year. You can use Any year as a valid entry.

    Start month

    Select a month for the exception event or Odd month , Even month , Any month .

    Day of month

    Select a value for the day of the month. You can use Any Day , Last day , Odd days or Even days as valid entries.

    Day of week

    Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

    Year

    Select a year. You can use Any year as a valid entry.

    Month

    Select a month for the exception event or Odd month , Even month , Any month .

  5. Click OK .

  • Edit Calendar Entry Dialog Box – Date Range
  • Calendar Editor Overview
  • General Information Properties – Basic Tab
  • References Tab