您可以编辑日期范围例外事件,以更改有关例外事件的信息。
在 WebStation 的 系统树 窗格中,选择包含您要编辑的日期范围例外事件的时间表。
点击 基本 选项卡。
在日历视图中,选择您要编辑的日期范围例外事件有效的日期。
在事件网格中,选择要编辑的日期范围例外事件。
点击 编辑时间表事件 按钮
在 时间表事件属性 对话框中,编辑属性。
Property |
Description |
Event type |
Click Exception to display the exception types. |
Exception type |
Select Date range for the exception to apply to the schedule. |
|
Click to add a line to the Times and values box. |
|
Click to delete an entry from the Times and values box. |
All Day |
Select to create an all day event. |
Name |
Type a name for the event. |
Priority |
Select a priority number between 1 (highest priority) and 16 (lowest priority). |
Year |
Select a year. You can use Any year as a valid entry. |
Month |
Select a month for the exception event or Odd month , Even month , Any month . |
Day of month |
Select a value for the day of the month. You can use Any Day , Last day , Odd days or Even days as valid entries. |
Day of week |
Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting. |
点击 确定 。