You use a panel to combine different viewable windows, for example, a graphic, trend chart, report, or another panel into a seamless view. A panel consists of one or several panes and one work area. The panel is available through the System Tree pane and opens as a window in the work area of the current workspace.
action_zoom_plus_stroke
图:
Example of panel components
In the procedure when creating a panel, you link existing objects to the panes or workspace that is added within the panel. Therefore you have to first create the object, for example a trend chart, before you add or rather link in the object into the panel. You can define whether to show or hide a pane's toolbar.
注释:
A panel cannot contain a System Tree.
A maximum of six levels of panels are allowed in a single pane, the recommendation for a good user experience is to only use three levels.
In a graphic or in the content of a pane or work area, you can create links that point to a panel. By using panels, you streamline the information you want to present to the user. For example, you have a graphic that represents a room. In the room illustration you add a fan symbol to which you link a panel containing panes and a work area that displays the current room airflow and temperature.