功能: 警报
产品版本: 1.8
2016/10/13

Editing an Action Note

You edit an existing action note to change the name or the descriptions, or to add the action note to another group.

To edit an action note
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Action notes .

  4. In the Action notes view, select the action note you want to edit .

     
    action_zoom_plus_stroke
  5. Click the Edit action note button

     
    action_zoom_plus_stroke
    .

    注释:
    • To permanently remove an action note from the action notes list, click the Remove action note button

       
      action_zoom_plus_stroke
      .

  6. In the Edit Action Note dialog box, in the Name box, type a name for the action note.

     
    action_zoom_plus_stroke
  7. In the Group name box, type a name to create a new group or select an existing group.

  8. In the Description box, type a description for the action note.

  9. Click OK .

  10. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Creating an Action Note
  • Alarm Control Panel – Action Notes View
  • Action Notes