Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Programaciones
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Editing an Event Priority

You edit an event priority to change the exception event to a higher or lower priority.

To edit an event priority
  1. In WorkStation, in the System Tree pane, right click the schedule you want to edit and click Open .

  2. In the Work area, click the Basic view of the Schedule editor.

  3. In the Event grid, select the exception event you want to edit.

  4. On the Basic toolbar, click the Edit schedule event button

     
    action_zoom_plus_stroke
    .

  5. In the S chedule Event Properties dialog box, in the Priority box, enter the priority level for the event.

  6. Click OK .

  • Priorities
  • Schedule Event Properties Dialog Box – Calculated Exception View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View