earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 1.9
2016/12/14

Editing the Software Permissions of a User Account Group

You edit the permissions of a path or commands that have been assigned to a user account group to configure the user account group's access in the Building Operation system.

显示更多
action_close

A user account group can comprise both user accounts and other user account groups with similar interests. By using a well planned strategy for your user account groups, you apply software ​permissions and polices to multiple user accounts.

For optimal efficiency, assign software permissions to user account groups rather than individual user accounts, wherever possible. Using this approach, you can associate user accounts to at least one user account group for controlled permission to Building Operation applications. For instance, you can group software permissions with user accounts based on common tasks and responsibilities​

You create user accounts groups and then apply one or more software permissions. For example, create a user account for Paul and associate him with the two user account groups: Administrators and Janitors. Paul inherits the software permissions of both user account groups. You can also set up general policies for the user accounts that are members to the user account group. For example, you can enable or disable the ability of group members to change their passwords or to close the User Interface. 有关更多信息,请参阅 Software Permissions .

 
action_zoom_plus_stroke Users inherit the user account group permissions of which they are members
图: Users inherit the user account group permissions of which they are members

Paul and Susan are members of the Janitor user account group, which includes an Operator workspace and a set of software permissions. The Janitor group is also a member of the Operator group. Therefore, the Janitor group inherits the settings and workspaces of the Operator group. In other words, Paul and Susan share the software permissions of both the Janitor and the Operator groups, and have access to the Operator and Janitor workspaces.

 
action_zoom_plus_stroke Software permissions and workspaces are assigned to user account groups
图: Software permissions and workspaces are assigned to user account groups

To edit the software permissions of a user account group
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Account management .

  4. In the Domain box, select the domain the user account group belongs to.

     
    action_zoom_plus_stroke
  5. In the User Account Groups box, select the user account group for which you want to edit the software permissions.

  6. Click Software permissions .

  7. Select the path for which you want to edit the user account permissions.

     
    action_zoom_plus_stroke
  8. In the Permission box, select the permission to the path.

     
    action_zoom_plus_stroke
  9. In the Category column, select a category that you want to configure permissions for.

  10. In the Command column, select a command.

  11. In the Permission box for the command, select a permission level.

     
    action_zoom_plus_stroke
  12. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Software Permissions and User Account Groups
  • Software Permissions
  • Assigning Software Permissions to a User Account Group
  • Removing Software Permissions from a User Account Group
  • Restricting the Permission to Change the Alarm State Sort Order
  • Control Panel View
  • User Account Group – Software Permissions Tab
  • Can not Access SmartStruxure Servers or Folders that You Earlier had Access to