earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WorkStation
Funktionaliteter: Larm
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-09-04

Enabling an Alarm

You enable alarms so they change state according to the variables the alarm monitors.

Visa mer
action_close

In the Alarms pane or Alarm View, you can disable an alarm. For example, you can disable an alarm if you need to do maintenance that you know will trigger the alarm.

Disabled alarms automatically disappear from the Alarms pane or Alarm View.

You can view disabled alarms to get information about the cause for disabling the alarm and the name of the user account that disabled the alarm.

Obs!
  • To disable an alarm that is in normal state, it is recommended that you use a connected shunt variable.

You enable disabled alarms so they once again change state according to the variables the alarms monitor.

 If you enable an alarm that has been disabled by a user (Disable cause = User), the alarm goes to Normal state for re-evaluation. If you enable an alarm that has been disabled by the System or a shunt variable, the alarm stays disabled.

To enable an alarm
  1. In WorkStation, in the Alarms pane or Alarm View, click the Show disabled alarms button

     
    action_zoom_plus_stroke
    .

  2. In the Alarms pane or Alarm View, right-click the alarm and then click Enable alarm .

If you enable an alarm that has been disabled by a user (Disable cause = User), the alarm goes to Normal state for re-evaluation. If you enable an alarm that has been disabled by the System or a shunt variable, the alarm stays disabled.

  • Disable and Enable Alarms
  • Disabling an Alarm
  • Alarms Pane and Alarm View
  • Alarms Pane and Alarm View Toolbar