earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WorkStation
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Enabling an Alarm

You enable alarms so they change state according to the variables the alarm monitors.

显示更多
action_close

In the Alarms pane or Alarm View, you can disable an alarm. For example, you can disable an alarm if you need to do maintenance that you know will trigger the alarm.

Disabled alarms automatically disappear from the Alarms pane or Alarm View.

You can view disabled alarms to get information about the cause for disabling the alarm and the name of the user account that disabled the alarm.

注释:
  • To disable an alarm that is in normal state, it is recommended that you use a connected shunt variable.

You enable disabled alarms so they once again change state according to the variables the alarms monitor.

 If you enable an alarm that has been disabled by a user (Disable cause = User), the alarm goes to Normal state for re-evaluation. If you enable an alarm that has been disabled by the System or a shunt variable, the alarm stays disabled.

Using WebStation you can display a list of all disabled alarms in the system. From the list you can enable the alarms.

有关更多信息,请参阅 Diagnostics in WebStation .

To enable an alarm
  1. In WorkStation, in the Alarms pane or Alarm View, click the Show disabled alarms button

     
    action_zoom_plus_stroke
    .

  2. In the Alarms pane or Alarm View, right-click the alarm and then click Enable alarm .

If you enable an alarm that has been disabled by a user (Disable cause = User), the alarm goes to Normal state for re-evaluation. If you enable an alarm that has been disabled by the System or a shunt variable, the alarm stays disabled.

  • Disable and Enable Alarms
  • Disabling an Alarm
  • Alarms Pane and Alarm View
  • Alarms Pane and Alarm View Toolbar