Productos WorkStation, Project Configuration Server
Funcionalidades: Alarmas
Versión del producto: 1.8
13/10/2016

Enabling State-Change Logging of an Alarm

You enable the state-change logging of an alarm.

Mostrar más
action_close

Every time an alarm changes its state, such as from alarm state to reset state, an event is written in the event log and shown in the Events pane in WorkStation. You can disable state-change logging if you are only interested in the current alarm status. For example, you want to present the current alarm status in a graphic and do not care about the event history.

Count

In the Alarm view, the value in the Count column counts +1 each time an alarm changes to alarm state. When the alarm state changes to normal, the count is reset to zero.

Para obtener más información, consulte Recuento .

To enable state-change logging of an alarm
  • ​In the Alarms pane or Alarm View, right-click the alarm you want to log and then click ​ Enable state-change logging .

  • Alarm State-Change Logging
  • Alarms Pane and Alarm View
  • Cómo ocultar una alarma
  • Cómo mostrar una alarma oculta
  • Cómo ver una alarma oculta
  • Deshabilitación de una alarma
  • Alarms Pane and Alarm View Toolbar